3. Timer configuration
In this step, you configure the timer.
Double-click the [Timer] from [Code Generator (Design Tool)] in the Project Tree. This opens the panel for the timer. |
Select the [General Setting] tab, and set the Channel0 to [Interval timer] . |
Select the [Channel 0] tab and make settings as shown below. |