Building a Program

Build the program you have created.

1. Build project

In this step, you save all the files being edited and the project, and rebuild the program.

Click the Save button.

Click the [Rebuild Project.] button.

Check to see if the rebuild process has been completed

correctly. If the build process has been completed correctly,

a load module file is created.

Tip

About setup of endian

The sample program used this time operates with the little endian.

If you want to use big endian, please change the endian following the instructions.

Select [Property] from [CC-RX(Build Tool)] in the Project Tree.

Make setting as shown below in Common Options.

If the message [Also change the endianness of the debug tool?] is outputted,please select [YES].