This section describes a procedure to create a program.
Start performing the task after installing CS+.
(3) Open the sample program :This time, you dont use the smart configurator functions. Instead, you must read out a program from a sample program. |
(4) Coding :Since you use a sample program, you dont edit the program. Here, we describe how to perform basic operations. |
(3) Build :Build the program (If an error occurs, edit the program again). |
(4) Debugging :Debug the program using RTK50565N2S10000BE and E2 Lite. |
(5) Writing : Write a program to the microcontroller using E2 Lite |