3. Plug-in setting
In this tutorial, the Smart Configurator functions are not used.
If you want to use the Smart Configurator functions, please check the plug-in setting by following the below procedure.
Select [Plug-in Setting] from the [Tool] menu. |
After configuring the settings as shown in the figure below, click [OK]. |
Select [Yes], then CS+ restarts. |