| 
 CS+ Update Manager window 
 | 
This window displays the status of and controls the update function.
Figure A.1  | CS+ Update Manager Window  | 
 
 
The following items are explained here.
[How to open]
-  | From the Windows [Start] menu, select [Programs] >> [Renesas Electronics CS+] >> [Update Manager].  | 
 
Remark  | In Windows 8.1, click on [Update Manager] on the start screen.  | 
 
-  | In the Windows task tray, click the  
 or balloon help (i).  | 
 
-  | From the CS+ [Help] menu, select [Check for Updates...].  | 
 
-  | From the Create Project dialog box of the CS+, click the [Update...] button.  | 
 
[Description of each area]
This area displays a menu for changing the appearance and settings of the main area.  Select an item to perform the corresponding action.
| 
 
All 
 | 
 
Displays the updates. 
 | 
| 
 
Microcontroller Name 
 | 
 
Displays the updates corresponding to that microcontroller. 
(Displays up to five microcontrollers for which the specify microcontroller function was used, most recent first.) 
 | 
| 
 
Download and install 
 | 
 
Downloads the selected updates, and after the downloads are complete, install them. 
 | 
| 
 
Download only 
 | 
 
Downloads the selected updates only. 
 | 
| 
 
Review update history 
 | 
 
Displays the update history. 
 | 
| 
 
Restore hidden updates	 
 | 
 
Displays the Restore hidden updates page. 
 | 
| 
 
Change settings	 
 | 
 
Displays the Update Manager Options dialog box. 
 | 
| 
 
Help 
 | 
 
Displays help. 
 | 
| 
 
Exit 
 | 
 
Exits Update Manager. 
 | 
 
Switch the display to one of the following pages, in accordance with the active function.