You can set specified items (columns) to always be displayed on the Function List panel/Variable List panel, even if the screen display is scrolled.
To do this, use the mouse to click the lock display icons ( 
  /  
 ) of the desired column name (clicking repeatedly toggles the item display between locked and unlocked).
Columns configured for locked display are locked at the leftmost column, so they will not be scrolled even if the user scrolls horizontally.
The meanings of the lock display icons are as follows:
You can also lock the display of a column by dragging and dropping it between two items with locked displays, or to the rightmost column.  |