2.7 Set Hex Output Options

To set options for the hex output phase, select the Build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.

You can set the various hex output options by setting the necessary properties in this tab.

Caution 1.

This tab is not displayed for the library project.

Caution 2.

This tab is displayed when you have selected [Always latest version which was installed] or V2.00.00 or a later version for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V2.00.00 or a later version of the CC-RX compiler has been installed.
When the version of the compiler package is V2.00.00 or lower, the properties from this tab are included in the [Convert Load Module File] category from the [Link Options] tab. See "Property panel" in "A. WINDOW REFERENCE" for details.

Remark

Often used options have been gathered under the [Frequently Used Options(for Hex Output)] category on the [Common Options] tab.