[Individual Assemble Options] tab


This tab shows the detailed information on an assemble source file categorized by the following and the configuration can be changed.

Note that this tab takes over the settings of the [Common Options] tab, [Compile Options] tab, and [Assemble Options] tab.

When the settings are changed from these tabs, the properties are displayed in boldface.

 

(1) [Debug Information]

(2) [Preprocess]

(3) [Output File]

(4) [Others]

Remark 1.

This tab is displayed only when [Yes] in the [Set individual assemble option] property in the [Build] category from the [Build Settings] tab is selected.

Remark 2.

For details on compiler driver options, refer to "MULTI: Building Applications for Embedded V850 and RH850" released by Green Hills Software, LLC. Please do not contact Green Hills Software, LLC with any inquiries about the CCRH850 build-tool plugin of CS+.

Caution

This tab is displayed only when the current project has been created with [Empty Application(GHS CCRH850)] or [Library(GHS CCRH850)] selected as the project type.

[Description of each category]

(1)

[Debug Information]

The detailed information on debug information is displayed and the configuration can be changed.

Debugging Level

Specify the -G option of the compiler driver.

Default

Configuration of the assemble option

How to change

Select from the drop-down list.

Restriction

MULTI(-G)

Specifies the -G option.

Not specify(No option specified)

Does not specify the -G option.

(2)

[Preprocess]

The detailed information on preprocessing is displayed and the configuration can be changed.

Include Directories

Specify the -I option of the compiler driver.

The following placeholders are supported.

%ActiveProjectDir%: Replaces with the absolute path of the active project folder.

%ActiveProjectName%: Replaces with the active project name.

%BuildModeName%: Replaces with the build mode name.

%MainProjectDir%: Replaces with the absolute path of the main project folder.

%MainProjectName%: Replaces with the main project name.

%MicomToolPath%: Replaces with the absolute path of the install folder of this product.

%ProjectDir%: Replaces with the absolute path of the project folder.

%ProjectName%: Replaces with the project name.

%TempDir%: Replaces with the absolute path of the temporary folder.

%WinDir%: Replaces with the absolute path of the Windows system folder.

The reference point of the path is the project folder.

The specified include path is displayed as the subproperty.

Uppercase characters and lowercase characters are not distinguished for the include paths.

Default

Include Directories[number of defined items]

How to change

Edit by the Path Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 247 characters

Up to 256 items can be specified.

Use whole include paths specified for build tool

Select whether to assemble using the include path specified in the [Include Directories] property in the [Preprocess] category from the [Assemble Options] tab of the build tool to be used.

The include paths are added by the following procedure.

-

Paths specified in the [Include Directories] property from this tab

-

Paths specified in the [Include Directories] property from the [Assemble Options] tab

-

Paths displayed in the [System include paths] property from the [Assemble Options] tab

This corresponds to the -I option of the compiler driver.

Default

Yes

How to change

Select from the drop-down list.

Restriction

Yes

Assembles using the include path specified in the property of the build tool to be used.

No

Does not use the include path specified in the property of the build tool to be used.

Define Preprocessor Symbol

Specify the -D option of the compiler driver.

Specify in the format of "macro name=defined value", with one macro name per line.

The specified macro is displayed as the subproperty.

Default

Define Preprocessor Symbol[number of defined items]

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 256 characters

Up to 256 items can be specified.

(3)

[Output File]

The detailed information on output files is displayed and the configuration can be changed.

Object file name

Specify the name of the object file generated after assembling.

The extension other than ".o" cannot be specified.

If the extension is omitted, ".o" is automatically added.

If this is blank, the file name will be the source file name with the extension replaced by ".o".

This corresponds to the -o option of the compiler driver.

Default

Blank

How to change

Directly enter in the text box.

Restriction

Up to 259 characters

(4)

[Others]

Other detailed information on assembly is displayed and the configuration can be changed.

Intermediate Forms of Output

Specify the -c option of the compiler driver.

Default

Configuration of the assemble option

How to change

Select from the drop-down list.

Restriction

Object File(-c)

Specifies the -c option.

Not specify(No option specified)

Does not specify the -c option.

Commands executed before assemble processing

Specify the command to be executed before assemble processing.

Use the call instruction to specify a batch file (example: call a.bat).

The following placeholders are supported.

%ActiveProjectDir%: Replaces with the absolute path of the active project folder.

%ActiveProjectName%: Replaces with the active project name.

%AssembledFile%: Replaces with the absolute path of the output file under assembling.

%BuildModeName%: Replaces with the build mode name.

%InputFile%: Replaces with the absolute path of the file to be assembled.

%MainProjectDir%: Replaces with the absolute path of the main project folder.

%MainProjectName%: Replaces with the main project name.

%MicomToolPath%: Replaces with the absolute path of the install folder of this product.

%Options%: Replaces with the command line option under build execution.

%OutputDir%: Replaces with the absolute path of the output folder.

%OutputFile%: Replaces with the absolute path of the output file.

%Program%: Replaces with the program name under execution.

%ProjectDir%: Replaces with the absolute path of the project folder.

%ProjectName%: Replaces with the project name.

%TempDir%: Replaces with the absolute path of the temporary folder.

%WinDir%: Replaces with the absolute path of the Windows system folder.

When "#!python" is described in the first line, the contents from the second line to the last line are regarded as the script of the Python console, and then executed before assemble processing.

The placeholders can be described in the script.

The specified command is displayed as the subproperty.

Default

Configuration of the assemble option

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 1023 characters

Up to 64 items can be specified.

Commands executed after assemble processing

Specify the command to be executed after assemble processing.

Use the call instruction to specify a batch file (example: call a.bat).

The following placeholders are supported.

%ActiveProjectDir%: Replaces with the absolute path of the active project folder.

%ActiveProjectName%: Replaces with the active project name.

%AssembledFile%: Replaces with the absolute path of the output file under assembling.

%BuildModeName%: Replaces with the build mode name.

%InputFile%: Replaces with the absolute path of the file to be assembled.

%MainProjectDir%: Replaces with the absolute path of the main project folder.

%MainProjectName%: Replaces with the main project name.

%MicomToolPath%: Replaces with the absolute path of the install folder of this product.

%Options%: Replaces with the command line option under build execution.

%OutputDir%: Replaces with the absolute path of the output folder.

%OutputFile%: Replaces with the absolute path of the output file.

%Program%: Replaces with the program name under execution.

%ProjectDir%: Replaces with the absolute path of the project folder.

%ProjectName%: Replaces with the project name.

%TempDir%: Replaces with the absolute path of the temporary folder.

%WinDir%: Replaces with the absolute path of the Windows system folder.

When "#!python" is described in the first line, the contents from the second line to the last line are regarded as the script of the Python console, and then executed after assemble processing.

The placeholders can be described in the script.

The specified command is displayed as the subproperty.

Default

Configuration of the assemble option

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 1023 characters

Up to 64 items can be specified.

Other additional options

Input the assemble option to be added additionally.

Add -asm= as required.

The options set here are added at the end of the assemble options group.

Default

Configuration of the assemble option

How to change

Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button.

Restriction

Up to 32767 characters