2.3 Set Compile Options

To set options for the compile phase, select the Build tool node on the project tree and select the [Compile Options] tab on the Property panel.

You can set the various compile options by setting the necessary properties in this tab.

Remark

Often used options have been gathered under the [Frequently Used Options(for Compile)] category on the [Common Options] tab.