| 
 | 
 | 
 | 
| 
 
E0592001 
 | 
 
Multiple input files are not allowed. 
 | 
 
Only one input file can be specified. 
Use the list file to specify multiple input files. 
 | 
| 
 
E0592002 
 | 
 
The option option cannot have an argument. 
 | 
 
An argument was specified for an option that should not have arguments. 
 | 
| 
 
E0592003 
 | 
 
The option option requires an argument. 
 | 
 
No argument was specified in an option that requires arguments. 
 | 
| 
 
E0592004 
 | 
 
The option option is specified more than once. 
 | 
 
Only one option can be specified at one time. 
 | 
| 
 
E0592005 
 | 
 
Requires an output file. 
 | 
 
The output file corresponding to the input file was not specified.  
 | 
| 
 
E0592006 
 | 
 
Failed to read an input file file. 
 | 
 
The folder name or file name may be incorrect. If the next file is specified in the list file, conversion of that file will start. 
 | 
| 
 
E0592007 
 | 
 
Failed to write a result of conversion file file. 
 | 
 
The folder name may be incorrect. 
 | 
| 
 
E0592008 
 | 
 
Failed to write an output file file. 
 | 
 
The folder name may be incorrect. 
 | 
| 
 
E0592009 
 | 
 
Failed to read a list file file. 
 | 
 
The folder name may be incorrect. 
 | 
| 
 
E0592010 
 | 
 
Syntax errors in list file file. 
 | 
 
The description of the list file is not correct. 
 | 
| 
 
E0592011 
 | 
 
File name is corrupted. 
 | 
 
There are duplicate file names among the input file, output file, and conversion result output file. 
 | 
| 
 
E0592012 
 | 
 
Invalid file name. 
 | 
 
Either the input file name specified on the command line or an input or output file name specified in the list file has exceeded 260 characters. 
 | 
| 
 
E0592013 
 | 
 
Invalid argument for the option option. 
 | 
 
The argument specification is invalid or the specified file name has exceeded 260 characters. 
 | 
| 
 
E0592101 
 | 
 
Illegal syntax in string. 
 | 
 
Conversion could not be performed because there was a syntax that is not allowed in the CA78K0. Modify the input file. 
 | 
| 
 
E0592102 
 | 
 
Can not add inline function for assembly. 
 | 
 
The number of inline functions for assembly has exceeded the upper limit. Modify the input file. 
 | 
| 
 
E0592103 
 | 
 
Failed to delete a temporary file. 
 | 
 
Deletion of a temporary file has failed. Delete the temporary file. 
 |