R_ADCn_ScanGroupm_GetResult


Reads the results of ADC scan group conversion.

[Syntax]

void    R_ADCn_ScanGroupm_GetResult ( uint16_t * buffer );

Remark

n is the unit number, m is the scan group number.

[Argument(s)]

I/O

Argument(s)

Description

O

uint16_t  * buffer;

Pointer to area in which to store the results of A/D conversion

[Return value]

None.