Renesas Electronics
r_csigm_callback_receiveend
Performs processing in response to the CSIG reception interrupt.
Remark
This API function is called as the callback routine of interrupt process r_csigm_interrupt_receive corresponding to the CSIG reception interrupt.
[Syntax]
void r_csigm_callback_receiveend ( void );
m is the channel number.
[Argument(s)]
None.
[Return value]