1.3 About RH850 Code Generator tool

The RH850 Code Generator tool has the following original spec.

 

-

Synchronization processing

The RH850 Code Generator tool output synchronization processing in Create and Stop of each peripherals. The user has to edit synchronization processing.

 

-

Interrupt vector table

The RH850 Code Generator tool can not edit interrupt vector table. When using generated interrupt function, please edit interrupt vector table.(Target device : RH850/E1L, E1M-S)

 

-

RH850 Code Generator sample project

The Code Generator install folder has SampleProjects folder. This folder has sample project.