Reads the results of A/D conversion (24 bits).
Remark The result of A/D conversion (24 bits) by this API function must be read within the maximum pending time of the ΔΣ A/D conversion result register n after ΔΣ A/D conversion end interrupt INTDSAD is generated.
[Syntax]
#include r_cg_macrodriver.h
void R_DSADC_Channeln_Get_Result ( uint32_t * const buffer );
Remark n is the channel number.
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 O  | 
 uint32_t * const buffer;  | 
 Pointer to area in which to store read results of A/D conversion  | 
[Return value]
None.