Count up to 100 falling edges.
[Waveform example]

[GUI setting example]
| 
 Timer  | 
 Used  | |||
| 
 TMRJ0  | 
 Used  | |||
| 
 Funcitons  | 
 Event counter mode  | |||
| 
 Count value  | 
 100  | |||
| 
 TRJIO0 input filter used  | 
 Unused  | |||
| 
 TRJIO0 event input  | 
 Always enable  | |||
| 
 TRJIO0 input polarity setting  | 
 One edge  | |||
| 
 TRJIO polarity switch setting  | 
 Starts counting at falling edge of the TRJIO0 input and TRJO0 starts output at H.  | |||
| 
 Enable output (TRJO0)  | 
 Unused  | |||
| 
 When the counter underflows, generate an interrupt(INTTRJ0)  | 
 Used  | |||
| 
 Priority  | 
 Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TMRJ0 counter */
R_TMR_RJ0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_timer_user.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_cnt = 0U;
/* End user code. Do not edit comment generated here */
static void __near r_tmr_rj0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Count INTTRJ0 */
g_cnt++;
/* End user code. Do not edit comment generated here */
}