r_bsc_buserr_interrupt

Performs processing in response to the bus error (illegal address access).

Remark 1. This API function is called to run interrupt processing for a bus error (illegal address access), which is generated through access by the processing program to a location within an illegal address range.

Remark 2. The bus master that caused the bus error can be confirmed by reading the MST bit of bus error status register 1 (BERSR1) from within this API function.

Remark 3. The illegal address (high-order 13 bits) that caused the bus error can be confirmed by reading the ADDR bit of bus error status register 2 (BERSR2) from within this API function.

[Syntax]

static void r_bsc_buserr_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.