r_cmpb_cmpbn_interrupt

Performs processing in response to the comparator B interrupt.

Remark This API function is called to run interrupt processing for the comparator Bn interrupt, which is generated when the comparison result changes at this time.

[Syntax]

static void r_cmpb_cmpbn_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.