R_CRC_Input_Data

Sets the initial value of the data from which the CRC is to be calculated.

[Syntax]

void R_CRC Input_Data ( uint8_t data );

void R_CRC Input_Data ( uint32_t data );

[Argument(s)]

I/O

Argument

Description

I

uint8_t data;

The initial value of the data from which the CRC is to be calculated

I/O

Argument

Description

I

uint32_t data;

The initial value of the data from which the CRC is to be calculated

Remark The size of argument differs for each device group.

[Return value]

None.