r_lvd_lvdn_interrupt

Performs processing in response to the voltage monitoring n interrupt.

Remark This API function is called to run interrupt processing for the voltage monitoring n interrupt, which is generated when the voltage detection circuit detects the voltage being dropped.

[Syntax]

static void r_lvd_lvdn_interrupt ( void );

Remark n is the circuit number.

[Argument(s)]

None.

[Return value]

None.