r_rtc_alm_interrupt

Performs processing in response to the alarm interrupt (ALM).

Remark This API function is called to run interrupt processing for the alarm interrupt (ALM), which is generated when the condition specified by R_RTC_Set_CalendarAlarm is satisfied.

[Syntax]

static void r_rtc_alm_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.