r_scifan_callback_error

Performs processing in response to the error interrupts.

Remark This API function is called as the r_scifan_erif_interrupt or r_scifan_brif_interrupt callback routine.

[Syntax]

static void r_scifan_callback_error ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.