r_tpu_tginm_interrupt

Performs processing in response to the input capture/compare match interrupt.

[Syntax]

static void r_tpu_tginm_interrupt ( void );

Remark m is the timer general register number, n is the channel number.

[Argument(s)]

None.

[Return value]

None.