2.5.7 Change creation date

The Code Generator is used to change the creation date into the file header of the source code by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Creation date] in the Property panel.

Figure 2.14

Change Output Destination Folder