Peripheral Functions panel


This panel allows you to configure the information necessary to control the peripheral functions (clock generator, port functions, etc.) provided.

Figure A.11

Peripheral Functions Panel

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Peripheral Functions] (>> Peripheral function node).

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Peripheral Functions] (>> Peripheral function node), and then press the [Enter] key.

-

From the [View] menu >> [Code Generator 2], select [Peripheral Functions].

 

Remark

If this panel is already open, pressing a different peripheral function button “ , , etc.” changes the content displayed in the Information setting area accordingly.

[Description of each area]

(1)

Toolbar

This area consists of the following “peripheral function buttons”.

When there is peripheral function target microcontroller is not supporting, peripheral functionbutton is not disokayed.

 

Outputs the source code (device driver program) to the folder specified by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Output folder] in the Property panel.

, , etc.

Changes the content displayed in the Information setting area to information required for controlling peripheral functions.

 

(2)

Information setting area

The content displayed in this area differs depending on the “peripheral function node” or “peripheral function button” selected or pressed when opening this panel.

See user’s manual for microcontroller for details on the items to be set.