CHAPTER 13 SYSTEM CONFIGURATION MANAGEMENT FUNCTIONS
The RI600PX's system configuration management function provides the function to reference the version information.
The version information can be referenced by issuing the following service call from the processing program.
- ref_ver, iref_ver
These service calls store the version information into the area specified by parameter pk_rver.
The following describes an example for coding these service calls.
Note 1 For details about the version information packet T_RVER, refer to "[Version information packet: T_RVER]".