This service call can be called from tasks that belong to Trusted Domain.
This service call deletes the variable-sized memory pool indicated by mplid.
When there are waiting tasks for the target variable-sized memory pool by using get_mpl or tget_mpl, this service call cancels the WAITING state of the tasks and returns E_DLT as a return value of the get_mpl or tget_mpl.