det_mem

Outline

Unregister memory object.

C format

 ER      det_mem (VP base);
Parameter(s)

I/O

Parameter

Description

I

 VP      base;
Memory object start address.



Explanation

This service call can be called from tasks that belong to Trusted Domain.

This service call unregisters the memory object started from the address specified by base.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_CTX

-25

Context error.

- This service call was issued in the CPU locked state.

- This service call was issued from non-task.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

E_MACV

-26

Memory access violation.

- Stack pointer points out of user stack for invoking task.

E_OACV

-27

Object access violation.

- The invoking task does not belong to trusted domain.

E_NOEXS

-42

Non-existent object.

- The memory object started from the address specified by base has already been registered.