-   
 
 pget_mpf
 ipget_mpf
 
-   
 
 Acquire fixed-sized memory block (polling).
 
 ER      pget_mpf (ID mpfid, VP *p_blk);
 ER      ipget_mpf (ID mpfid, VP *p_blk);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      mpfid;
 
 | 
 ID number of the fixed-sized memory pool.
  
 | 
| 
 | 
 VP      *p_blk;
 
 | 
 Start address of the acquired memory block.
  
 | 
 
 This service call acquires the fixed-sized memory block from the fixed-sized memory pool specified by parameter 
mpfid and stores the start address in the area specified by parameter 
p_blk.
 
 If a fixed-sized memory block could not be acquired from the target fixed-sized memory pool (no available fixed-sized memory blocks exist) when this service call is issued, fixed-sized memory block acquisition processing is not performed but "E_TMOUT" is returned.
 
 Note 1	 The contents of the block are undefined.
 
 Note 2	 The alignment number of memory block is 1. Please perform the following, in order to enlarge the alignment number of memory blocks.
 
 -	 Specify the memory block size to a multiple of the desired alignment number at creating the fixed-sized memory pool.
 
 -	 Make the start address of the fixed-sized memory pool area into the address of the desired alignment number.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 Note	 When the ipget_mpf is issued from task or the pget_mpf is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
  
 | 
| 
 | 
 | 
 Memory access violation. (only for pget_mpf)
  
 -	 Stack pointer points out of user stack for invoking task.
  
 -	 The operand-write access to the area indicated by  p_blk has not been permitted to the invoking task.
  
 | 
| 
 | 
 | 
 -	 The fixed-sized memory pool specified by  mpfid does not exist.
  
 | 
| 
 | 
 | 
 |