-   
 
 snd_mbx
 isnd_mbx
 
-   
 
 ER      snd_mbx (ID mbxid, T_MSG *pk_msg);
 ER      isnd_mbx (ID mbxid, T_MSG *pk_msg);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      mbxid;
 
 | 
 ID number of the mailbox.
  
 | 
| 
 | 
 T_MSG   *pk_msg;
 
 | 
 Start address of the message packet to be sent to the mailbox.
  
 | 
 
 [Message packet T_MSG for TA_MFIFO attribute]
 
 
 typedef struct {
     VP      msghead;       /*RI600PX management area*/
 } T_MSG;
 
 | 
 
 [Message packet for T_MSG_PRI for TA_MPRI attribute]
 
 
 typedef struct {
     T_MSG   msgque;        /*Message header*/
     PRI     msgpri;        /*Message priority*/
 } T_MSG_PRI;
 
 | 
 
 This service call transmits the message specified by parameter 
pk_msg to the mailbox specified by parameter 
mbxid (queues the message in the wait queue).
 
 If a task is queued to the target mailbox wait queue when this service call is issued, the message is not queued but handed over to the relevant task (first task of the wait queue).
 
 As a result, the relevant task is unlinked from the wait queue and is moved from the WAITING state (receiving WAITING state for a mailbox) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
 
 Note 1	 Messages are queued to the target mailbox message queue in the order specified at creating the mailbox (FIFO order or message priority order).
 
 Note 2	 Do not modify transmitted message (the area indicated by 
pk_msg) until the message is received.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 When the target mailbox has TA_MPRI attribute:
  
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 The isnd_mbx was issued from task.
  
 -	 The snd_mbx was issued from non-task.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 | 
| 
 | 
 | 
 Memory access violation. (only for snd_mbx)
  
 -	 Stack pointer points out of user stack for invoking task.
  
 -	 The operand-read and operand-write access to the message header area has not been permitted to the invoking task. Message header area:
  
 -	 TA_MFIFO attribute : The T_MSG structure started from the address indicated by pk_msg
  
 -	 TA_MPRI attribute : The T_MSG_PRI structure started from the address indicated by pk_msg
  
 | 
| 
 | 
 | 
 -	 The mailbox specified by  mbxid does not exist.
  
 |