-   
 
 prcv_mbx
 iprcv_mbx
 
-   
 
 Receive from mailbox (polling).
 
 ER      prcv_mbx (ID mbxid, T_MSG **ppk_msg);
 ER      iprcv_mbx (ID mbxid, T_MSG **ppk_msg);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      mbxid;
 
 | 
 ID number of the mailbox.
  
 | 
| 
 | 
 T_MSG   **ppk_msg;
 
 | 
 Start address of the message packet received from the mailbox.
  
 | 
 
 [M[Message packet T_MSG for TA_MFIFO attribute ]
 
 
 typedef struct {
     VP      msghead;       /*RI600V4 management area*/
 } T_MSG;
 
 | 
 
 [Message packet T_MSG_PRI for TA_MPRI attribute]
 
 
 typedef struct {
     T_MSG   msgque;        /*Message header*/
     PRI     msgpri;        /*Message priority*/
 } T_MSG_PRI;
 
 | 
 
 This service call receives a message from the mailbox specified by parameter 
mbxid, and stores its start address in the area specified by parameter 
ppk_msg.
 
 If the message could not be received from the target mailbox (no messages were queued in the wait queue) when this service call is issued, message reception processing is not executed but "E_TMOUT" is returned.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 Note	 When the iprcv_mbx is issued from task or the prcv_mbx is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
  
 | 
| 
 | 
 | 
 |