-   
 
 rcv_dtq
 
-   
 
 Receive from data queue (waiting forever).
 
 ER      rcv_dtq (ID dtqid, VP_INT *p_data);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      dtqid;
 
 | 
 ID number of the data queue.
  
 | 
| 
 | 
 VP_INT  *p_data;
 
 | 
 Data element received from the data queue.
  
 | 
 
 This service call processes as follows according to the situation of the data queue specified by the parameter 
dtqid.
 
 -	 There is a data in the data queue.
This service call takes out the oldest data from the data queue and stores the data to the area specified by 
p_data.
When there is a task in the transmission wait queue, this service call stores the data sent by the task in the top of the transmission wait queue and moves it from the WAITING state (data transmission wait state) to the READY state.
 
 -	 There is no data in the data queue and there is a task in the transmission wait queue.
This service call stores the data specified by the task in the top of the transmission wait queue to the area specified by 
p_data. As a result, the task is unlinked from the transmission wait queue and moves from the WAITING state (data transmission wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
Note, this situation is caused only when the capacity of the data queue is 0.
 
 -	 There is no data in the data queue and there is no task in the transmission wait queue.
This service call queues the invoking task to the reception wait queue of the target data queue and moves it from the RUNNING state to the WAITING state (data reception wait state). 
The receiving WAITING state for a data queue is cancelled in the following cases.
 
 
 Receiving WAITING State for a Data Queue Cancel Operation
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  snd_dtq.
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  psnd_dtq.
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  ipsnd_dtq.
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  tsnd_dtq.
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  fsnd_dtq.
  
 | 
 | 
 Data was sent to the data queue area as a result of issuing  ifsnd_dtq.
  
 | 
 | 
 Forced release from waiting (accept  rel_wai while waiting).
  
 | 
 | 
 Forced release from waiting (accept  irel_wai while waiting).
  
 | 
 | 
 
 Note	 Invoking tasks are queued to the reception wait queue of the target data queue in the order of the data reception request.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued from a non-task.
  
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the dispatching disabled state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 | 
| 
 | 
 | 
 Forced release from the WAITING state.
  
 |