-
ref_ver
iref_ver
-
Reference version information.
ER ref_ver (T_RVER *pk_rver);
ER iref_ver (T_RVER *pk_rver;
|
|
|
|
|
|
T_RVER *pk_rver;
|
Pointer to the packet returning the version information.
|
[Version information packet: T_RVER]
typedef struct t_rver {
UH maker; /*Kernel maker code*/
UH prid; /*Identification number of the kernel*/
UH spver; /*Version number of the ITRON specification*/
UH prver; /*Version number of the kernel*/
UH prno[4]; /*Management information of the kernel*/
} T_RVER;
|
These service calls store the RI600V4 version information into the area specified by parameter pk_rver.
-
maker
The
maker represents the manufacturer who created this kernel. In the RI600V4, 0x011B, which is the maker code assigned for Renesas Electronics Corporation, is returned for maker.
Note, the value defined in the kernel configuration macro
TKERNEL_MAKER is same as
maker.
-
prid
The
prid represents the number that identifies the kernel and VLSI. In the RI600V4, 0x0003 is returned for
prid.
Note, the value defined in the kernel configuration macro
TKERNEL_PRID is same as
prid.
-
spver
The
spver represents the specification to which this kernel conforms. In the RI600V4, 0x5403 is returned for
spver.
Note, the value defined in the kernel configuration macro
TKERNEL_SPVER is same as
spver.
-
prver
The
prver represents the version number of this kernel.
For example, 0x0123 is returned for
prver when the kernel version is "V1.02.03".
Note, the value defined in the kernel configuration macro
TKERNEL_PRVER is same as
prver.
-
prno
The
prno represents product management information and product number, etc. In the RI600V4, 0x0000 is returned for all
prnos.
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued in the CPU locked state.
- This service call was issued in the status PSW.IPL > kernel interrupt mask level.
Note When the iref_ver is issued from task or the ref_ver is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
|