-   
 
 rsm_tsk
 irsm_tsk
 
-   
 
 ER      rsm_tsk (ID tskid);
 ER      irsm_tsk (ID tskid);
 These service calls move the task specified by parameter 
tskid from the SUSPENDED state to the READY state, or from the WAITING-SUSPENDED state to the WAITING state.
 
 Note 1	 These service calls do not perform queuing of forced cancelation requests. If the target task is neither in the SUSPENDED state nor WAITING-SUSPENDED state, "E_OBJ" is returned.
 
 Note 2	 The RI600V4 does not support queuing of suspend request. The behavior of the 
frsm_tsk and 
ifrsm_tsk, that can release from the SUSPENDED state even if suspend request has been queued, are same as 
rsm_tsk and 
irsm_tsk.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 The irsm_tsk was issued from task.
  
 -	 The rsm_tsk was issued from non-task.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 | 
| 
 | 
 | 
 -	 Specified task is neither in the SUSPENDED state nor WAITING-SUSPENDED state.
  
 |