-   
 
 sta_cyc
 ista_cyc
 
-   
 
 Start cyclic handler operation.
 
 ER      sta_cyc (ID cycid);
 ER      ista_cyc (ID cycid);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      cycid;
 
 | 
 ID number of the cyclic handler.
  
 | 
 
 This service call moves the cyclic handler specified by parameter 
cycid from the non-operational state (STP state) to operational state (STA state).
 
 As a result, the target cyclic handler is handled as an activation target of the RI600V4.
 
 -	 When the TA_PHS attribute is specified
The target cyclic handler activation timing is set up according to 
Activation phase (phs_counter) and 
Activation cycle (interval_counter).
If the target cyclic handler has already been started, however, no processing is performed even if this service call is issued, but it is not handled as an error.
 
 -	 When the TA_PHS attribute is not specified
The target cyclic handler activation timing is set up according to 
Activation cycle (interval_counter)) on the basis of the call time of this service call.
This setting is performed regardless of the operating status of the target cyclic handler.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 Note	 When the ista_cyc is issued from task or the sta_cyc is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
  
 |