-   
 
 tget_mpl
 
-   
 
 Acquire variable-sized memory block (with time-out).
 
 ER      tget_mpl (ID mplid, UINT blksz, VP *p_blk, TMO tmout);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      mplid;
 
 | 
 ID number of the variable-sized memory pool.
  
 | 
| 
 | 
 UINT    blksz;
 
 | 
 Memory block size to be acquired (in bytes).
  
 | 
| 
 | 
 VP      *p_blk;
 
 | 
 Start address of the acquired memory block.
  
 | 
| 
 | 
 TMO     tmout;
 
 | 
 Specified time-out (in millisecond).
  
 Value:	Specified time-out.
  
 | 
 
 This service call acquires a variable-size memory block of the size specified by parameter 
blksz from the variable-size memory pool specified by parameter 
mplid, and stores its start address into the area specified by parameter 
p_blk.
 
 If no variable-size memory blocks could be acquired from the target variable-size memory pool (no successive areas equivalent to the requested size were available) when this service call is issued, this service call does not acquire variable-size memory blocks but queues the invoking task to the target variable-size memory pool wait queue and moves it from the RUNNING state to the WAITING state with time-out (variable-size memory block acquisition wait state).
 
 The WAITING state for a variable-sized memory block is cancelled in the following cases.
 
 
 WAITING State for a Variable-sized Memory Block Cancel Operation
  
 | 
 | 
 The variable-size memory block that satisfies the requested size was returned to the target variable-size memory pool as a result of issuing  rel_mpl.
  
 | 
 | 
 The task at the top of the transmission wait queue was forcedly released from waiting by following either.
  
 -	 Forced release from waiting (accept  rel_wai while waiting).
  
 -	 Forced release from waiting (accept  irel_wai while waiting).
  
 -	 Forced release from waiting (accept  ter_tsk while waiting).
  
 -	 The time specified by  tmout for  tget_mpl has elapsed.
  
 | 
 | 
 Forced release from waiting (accept  rel_wai while waiting).
  
 | 
 | 
 Forced release from waiting (accept  irel_wai while waiting).
  
 | 
 | 
 The variable-sized memory pool is reset as a result of issuing  vrst_mpl.
  
 | 
 | 
 The time specified by  tmout has elapsed.
  
 | 
 | 
 
 Note 2	 Invoking tasks are queued to the target variable-size memory pool wait queue in the FIFO order.
 
 Note 3	 The contents of the block are undefined.
 
 Note 5	 
TMO_FEVR is specified for wait time 
tmout, processing equivalent to 
get_mpl will be executed. When 
TMO_POL is specified, processing equivalent to 
pget_mpl will be executed.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 blksz  exceeds the maximum size that can be acquired.
 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued from a non-task.
  
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the dispatching disabled state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 | 
| 
 | 
 | 
 Forced release from the WAITING state.
  
 | 
| 
 | 
 | 
 Polling failure or specified time has elapsed.
  
 | 
| 
 | 
 | 
 Released from WAITING state by the object reset ( vrst_mpl)
  
 |