-
Property panel
-
This panel is used to display information regarding the node selected on the Project Tree panel and change the settings of the information.
This panel can be opened as follows:
-
On the Project Tree panel, select a component such as the Realtime OS node or the system configuration file, and then select the [View] menu -> Property] or select [Property] from the context menu.
Note When the Property panel is already open, selecting a component such as the Realtime OS node or the system configuration file on the
Project Tree panel displays the detailed information regarding the selected component.
When multiple nodes are selected, this area is blank.
2 ) Detailed information display/change area
In this area, the detailed information on the Realtime OS node, system configuration file, or the like that is selected on the
Project Tree panel is displayed by every category in the list. And the settings of the information can be changed directly.
Mark

indicates that all the items in the category are expanded. Mark

indicates that all the items are collapsed. You can expand/collapse the items by clicking these marks or double clicking the category name.
See the section on each tab for the details of the display/setting in the category and its contents.
3 ) Property description area
Display the brief description of the categories and their contents selected in the detailed information display/change area.
Categories for the display of the detailed information are changed by selecting a tab.
In this panel, the following tabs are contained (see the section on each tab for the details of the display/setting on the tab).
- [Category Information] tab
- When the system information table file or entry file is selected on the
Project Tree panel
- [Individual Assemble Options] tab
- [Individual Assemble Options] tab
Note1 See "CS+ CC-RH Build Tool Operation" for details about the [File Information], [Category Information], [Build Settings], [Individual Assemble Options], and [Individual Compile Options] tabbed pages.
Note2 When multiple components are selected on the
Project Tree panel, only the tab that is common to all the components is displayed. If the value of the property is modified, that is taken effect to the selected components all of which are common to all.