This option specifies the folder to search include files.
[Specification format]
- | Interpretation when omitted |
The include file is searched from the standard include file folder.
[Detailed description]
- | This option specifies the folder to search include files which are read by preprocessor directive "#include"or assembler control instruction "$INCLUDE/$BINCLUDE" as path.
Include files are searched according to the following sequence.
|
(a) | Folder with source files (When files are specified by using " ") |
(b) | Path specified by the -I option |
(c) | Standard include file folder |
(a) | Path specified by the -I option |
(b) | Folder with source file |
- | If path does not exist, a warning will be output. |
- | An error will occur if path is omitted. |
[Example of use]
- | To search include files from the current folder, folder D:\include, the standard folder in that order, describe as: |
>ccrh -ID:\include -Xcommon=rh850 main.c
|