This option specifies the mode for rounding floating-point constants.
Floating-point constants are rounded to the nearest representable values (this is the same result as when -Xround=nearest is specified).
If this option is specified together with the -Xfloat=soft option, this option will be invalid and floating-point constants will always be rounded to the nearest representable values. |