This option displays the version information of asrh.
[Specification format]
- | Interpretation when omitted |
Assembling is performed without displaying the version information of asrh.
[Detailed description]
- | This option outputs the version information of asrh to the standard error output.
It does not execute assembling.
|
[Example of use]
- | To output the version information of asrh to the standard error output, describe as: |