The predefined macro names in CC-RH are listed below.
Table 4.8 | List of Supported Macros |
|
|
|
At all times
|
__LINE__
|
Line number of source line at that point (decimal)
|
At all times
|
__FILE__
|
Name of source file (character string constant)
|
At all times
|
__DATE__Note 2
|
Date of translating source file (character string constant)Note 3
|
At all times
|
__TIME__Note 2
|
Translation time of source file (character string constant)Note 4
|
When -strict_std is specified
|
__STDC__
|
1
|
When -lang=c99 is specified
|
__STDC_HOSTED__
|
0
|
At all times
|
__STDC_VERSION__
|
199409L (when -lang=c99 is not specified)
199901L (when -lang=c99 is specified)
|
When -lang=c99 is specified
|
__STDC_IEC_559__
|
1
|
At all times
|
__RENESAS__
|
1
|
At all times
|
__RENESAS_VERSION__
|
0xXXYYZZ00Note 5
|
At all times
|
__CCRH__
|
1
|
__CCRH
|
1
|
At all times
|
__RH850__
|
1
|
__RH850
|
1
|
At all times
|
__v850e3v5__
|
1
|
__v850e3v5
|
1
|
When -Xdbl_size=4 is specified
|
__DBL4
|
1
|
__DOUBLE_IS_32BITS__
|
1
|
When -Xdbl_size=8 is specified
|
__DBL8
|
1
|
__DOUBLE_IS_64BITS__
|
1
|
When -Xround=nearest is specified
|
__RON
|
1
|
When -Xround=zero is specified
|
__ROZ
|
1
|
When -Xbit_order=left is specified
|
__BITLEFT
|
1
|
When -Xbit_order=right is specified
|
__BITRIGHT
|
1
|
When -Xenum_type=auto is specified
|
__AUTO_ENUM
|
1
|
When -Xfloat=fpu is specified
|
__FPU
|
1
|
At all times
|
__CHAR_SIGNED__
|
1
|
When -Xreg_mode=32 is specified
|
__reg32__
|
1
|
When -Xreg_mode=22 is specified
|
__reg22__
|
1
|
When -Xreg_mode=common is specified
|
__reg_common__
|
1
|
At all times
|
_LIT
|
1
|
When -Xmulti_level=level is specified
|
__MULTI_LEVEL__
|
Value specified by level (decimal)
|
When -pic is specified
|
__PIC
|
1
|
When -pirod is specified
|
__PIROD
|
1
|
When -pid is specified
|
__PID
|
1
|
Note 1. | The condition specified by the option is applicable also for the interpretation when the option is omitted. |
Note 2. | The date and time of translation can be obtained in any case; the __DATE__ and __TIME__ macro values are always defined. |
Note 3. | Character string constant in the form of "Mmm dd yyyy". Here, the name of the month (Mmm) is the same as that generated by the asctime function stipulated by the C language standard (three alphabetic characters with only the first character being a capital letter). The first character of dd is blank if its value is less than 10. |
Note 4. | Character string constant having a format of "hh:mm:ss" similar to the time created by the asctime function. |
Note 5. | If the version is V.XX.YY.ZZ, this will be 0xXXYYZZ00.
Example V1.02.03 -> __RENESAS_VERSION__ = 0x01020300
|