Initialization of 4-byte area.
The .db4 and .dw directive tells the assembler to initialize a memory area in 4-byte units with the initial value(s) specified in the operand field. |
Use the .db4 and .dw directive when defining a 4-byte numeric constant such as an address or data used in the program. |
The value of an expression must be 4-byte data. Therefore, the value of the operand must be in the range of 0x0 to 0xFFFFFFFF. If the value exceeds 4-byte, the assembler will use only lower 2-byte of the value as valid data.
No character string constants can be described as an initial value.
As an initial value, an expression that includes a relocatable symbol or external reference symbol may be described. |
If the relocation attribute of the section containing the .db4 and .dw directive is "BSS", then an error is output because initial values cannot be specified. |