This option specifies the address range of the mirror destination area.
[Specification format]
-mirror_region=start_address,end_address
|
- | Interpretation when omitted |
When the -dev option is not specified, a device without a mirror area is assumed.
[Detailed description]
- | This option specifies the address range (start address and end address) of the mirror destination area. |
- | This option is used to calculate the address range of the mirror source area.
0xF8000 is subtracted from the specified addresses when the CPU core type is RL78-S1, or 0xF0000 is subtracted when the CPU core type is RL78-S2 or RL78-S3. The obtained addresses are assumed as the address range of the mirror source area. If a value outside the range from 0xF0000 to 0xFFFFF is specified, an error will occur.
|
- | If both the -dev option and this option are specified, an error will occur. |
- | When the -cpu option is specified but this option is not specified, a device without a mirror area is assumed. |
- | When both the -mirror_source=common option and this option are specified, an error will occur. |
[Example of use]
- | To specify the address range of the mirror destination area. |
>asrl -cpu=S2 -mirror_region=0xf3000,0xfaeff main.asm
|