This option specifies the notation of the radix for numeric constants.
[Specification format]
-base_number={prefix|suffix}
|
- | Interpretation when omitted |
It is the same result as when the -base_number=prefix option is specified.
[Detailed description]
- | This option specifies the notation of the radix for numeric constants. |
- | The parameters that can be specified are shown below.
An error will occur if any other item is specified.
|
prefix
|
Specifies the prefix notation (0xn...n).
|
suffix
|
Specifies the suffix notation (n...nH).
|
- | An error will occur if the parameter is omitted. |
[Example of use]
- | To specify the suffix notation of the radix for numeric constants, describe as: |
>asrl -base_number=suffix -dev=dr5f100pj.dvf main.asm
|