This option specifies the output format.
A load module file is output (It is the same result as when the -form=absolute option is specified).
|
Use this when a module is extracted as an object file from a library by the -extract option. |
|
|
When "library=s" is specified, a system library file is output. When "library=u" is specified, a user library file is output. If only "library" is specified, it is assumed that "library=u" has been specified. |
|
|
See "3.5 Intel HEX File" for details. |
|
|
Outputs a Motorola S-record file. See "3.6 Motorola S-record File" for details. |
|
The following options can always be specified. |
The -byte_count option is valid only when the -form=hexadecimal or -form=stype option is specified. |
If an Intel HEX file is specified as an input file, only the -form=hexadecimal option can be specified. If a Motorola S-record file is specified, only the -form=stype option can be specified. |
The -fix_record_length_and_align option is valid only when the -form=hexadecimal or -form=stype option is specified. |
The -check_output_rom_area option is valid only when the -form=hexadecimal or -form=stype option is specified. |