This option disables checking of the address to which the section is allocated.
[Specification format]
- | Interpretation when omitted |
Whether sections are allocated to memory as shown below is checked, and if they are not allocated so, an error will occur.
|
|
|
|
.option_byte
|
Address is fixed
|
|
.security_id
|
Address is fixed
|
|
.sbss / .sdata
|
saddr area
|
|
.sbss / .sdata (RAM side when the -rom option is specified)
|
saddr area
|
|
.bss / .data
|
Internal RAM
|
|
.bss / .data (RAM side when the -rom option is specified)
|
Internal RAM
|
|
.const
|
Flash mirror space
|
|
.constf
|
Internal ROM
|
|
.sdata / .data (ROM side when the -rom option is specified)
|
Internal ROM
|
|
.text
|
Program memory
|
|
.text_unit64kp / .textf
|
Program memory
|
[Detailed description]
- | This option disables checking whether the memory location that is read from the device file is consistent with the memory location of the section. |
[Example of use]
- | To disable checking of the address to which the section is allocated, describe as: |
>rlink a.obj b.obj -no_check_section_layout
|
[Remark]
- | If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |