4.1 Basic Language Specifications

This section explains the implementation-defined behavior of the CC-RL which is compliant with the C90 and C99 standards.

See "4.2 Extended Language Specifications" for extended language specifications explicitly added by the CC-RL.