The following table lists the names, relocation attribute of these reserved sections.
Table 6.1 | Reserved Sections |
|
|
|
|
|
.callt0
|
CALLT0
|
Section for the table to call the callt function
|
|
.text
|
TEXT
|
Section for code (allocated to the near area)
|
|
.textf
|
TEXTF
|
Section for code (allocated to the far area)
|
|
.textf_unit64kp
|
TEXTF_UNIT64KP
|
Section for code (section is allocated so that the start address is an even address and the section does not exceed the (64 Kbytes - 1) boundary)
|
|
.const
|
CONST
|
ROM data (allocated to the near area) (within the mirror area)
|
|
.constf
|
CONSTF
|
ROM data (allocated to the far area)
|
|
.data
|
DATA
|
Section for near initialized data (with initial value)
|
|
.dataf
|
DATAF
|
Section for far initialized data (with initial value)
|
|
.sdata
|
SDATA
|
Section for initialized data (with initial value, variable allocated to saddr)
|
|
.bss
|
BSS
|
Section for data area (without initial value, allocated to the near area)
|
|
.bssf
|
BSSF
|
Section for data area (without initial value, allocated to the far area)
|
|
.sbss
|
SBSS
|
Section for data area (without initial value, variable allocated to saddr)
|
|
.option_byte
|
OPT_BYTE
|
Section specific for user option byte and on-chip debugging specificatio
|
|
.security_id
|
SECUR_ID
|
Section specific for security ID specification
|
|
.vect<vector table address>Note
|
AT
|
Interrupt vector table
If the -split_vect option is specified, a section is generated based on ".vect<vector table address>". The vector table address is in hexadecimal notation.
|
The default section name can be changed using #pragma section.
Note | Cannot be changed by #pragma section. |