11.1.6 MISRA2004 check (rule number 10.1)
Unnecessary message may be output for statements with enumerated-type variables, return statements with
enumerated-type return values, or statements with enumerators in a file satisfying the following conditions (1), (2), and (3).
(1) | Option -signed_char is not specified and enumerated-type definitions whose range of enumerator value is within a range of 0 to 255 are included,
or
option -signed_char is specified and enumerated-type definitions whose range of enumerator value is within a range of -128 to 255 are included.
|
(2) | Statements with enumerated-type variables, return statements with enumerated-type return values, or statements with enumerators are included. |
(3) | MISRA check option against rule 10.1 is specified. |
typedef enum E { E1 = 0, E2, E3 } etype;
etype func( void );
etype evar;
etype func(void)
{
evar = E1; // Message against rule 10.1 is output.
return E1; // Message against rule 10.1 is output.
}
|
(Workaround)
Cast enumerators to enumerated type.
typedef enum E { E1 = 0, E2, E3 } etype;
etype func( void );
etype evar;
etype func(void)
{
evar = (etype)E1; // Cast enumerator E1 to etype
return (etype)E1; // Cast enumerator E1 to etype
}
|