-nobank [V3.01.00 or later]


< Assembler Command Options / Object Options >

[Format]

-nobank

 

-

Interpretation when omitted

When the CPU*1 is selected or RXv1 or RXv2 is selected as ISA*2, -nobank is assumed to be specified.

In other cases, -bank is assumed to be specified.

Note

*1) This means a selection by the cpu option or the CPU_RX environment variable.

*2) This means a selection by the isa option or the ISA_RX environment variable.

[Description]

-

This option generates an error when the SAVE or RSTR instruction dedicated to the register bank save function is written.