< Assembler Command Options / List Options >
If this option is not specified, no assemble list file is output.
When the listfile option is specified, an assemble list file is output. The name of the file can also be specified. |
If <file name> is not specified in the listfile option, the source file name with the extension replaced with .lst is used as the source list file name. |